DRV.NVSAVE
Description
DRV.NVSAVE saves the current drive parameter values from the RAM to the NV memory.
The drive parameters that were saved to the NV are read from the NV on the next drive boot, causing the values to be automatically set to the saved values on every drive boot.
Executing DRV.RSTVAR does not modify the values of the NV, but instead sets the drive values in RAM to their defaults.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
DRV.NVSAVE | 0x3000 | 0x4 | UDINT | - | - | wo | False |